Post Go back to editing

Place channels in parallel to increase max current

Category: Datasheet/Specs
Product Number: MAX25512

Can I tie multiple channels together to increase the "max current" I can draw in an LED string? Say if I tie channel 1 and 2 together to control a higher power LED string. Would I then have a current control range between 0-240mA? For example, I can get around 180mA by setting one channel to 120mA and the other to 60mA.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.