LTC4267
Production
The LTC4267 combines an IEEE 802.3af compliant Powered Device (PD) interface with a current mode switching regulator, providing a complete power solution...
Datasheet
LTC4267 on Analog.com
Hello, ADI Team
I am using the 5V non-isolated circuit provided in the datasheet to power my board,
but I had to change the transformer to Bourns 'POE060-FD20120S' due to supply issues during development.
Using the attached schematic, I fabricated several boards for testing,
and 20-30% of them exhibited issues with the PoE section.
The problematic boards were operated for several minutes, then the power supply stopped along with a noise sound,
and the MMBTA42 (Q1) transistor was found to be damaged.
There might be additional issues in other parts, but it is difficult to check them with the equipment I currently have.
I would like to know if there are any circuit modifications needed to accommodate the substituted transformer,
or if this transformer is simply not suitable for use with the LTC4267.
If this transformer is not suitable, I would appreciate it if you could recommend an alternative transformer that I could use.
Thank you for your time and assistance.

Hello,
My apologies for the delayed response. I would change D4 to an 9.1V zener diode. Per the LTC4267 datasheet, you should keep any low impedance sources such as the regulator based on Q1 to 8V or less. The SMAJ9.0A is a TVS, so its specified for around 10V - 11V at 1mA, up to 15V at higher currents. It's possibly your design exceeded 8V at PVCC so the internal clamp overloaded Q1.
I briefly looked at your transformer and it should work, though it seems a bit beefy for the LTC4267's power level. You could can find an EP13 or even EP7 for 13W designs.
Best Regards,
Eric