Post Go back to editing

Unable to write the register

Category: Software
Product Number: MAX20480

I am using the MAX20480 as per below schematic in one of my project for voltage monitoring.

I am able to read the registers as below, Able to read the correct CID, I2C address. And default register values as per datasheet.

I am unable to write the any read/write register. We want to set the nominal voltage to 2.5V for IN3, IN4 and IN5, 0.9V for IN1 and 1.65V for IN2. Also over voltage to 105% and undervoltage to 95%. Unable to do this. Please help me to solve this issue.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.