Hi
I use ADP5070 and LT3032 to create +/-5.5V output.
If I disconnect the LT3032 output by remove B1 ,B2 , I can get +/- 5V output .

I put a 47R resister R54 to the +5.5V output , the ADP5070 output waveform as follows.

I need ADP5070 output at least +/- 150mA to drive LT3032, but it cannot work well.
How should I do to get enough output current ?
Thanks
Cong