Post Go back to editing

Current In maximum ratings

Category: Hardware
Product Number: LTC3588-1

I am interested in continuous higher power harvesting. PZ1 & PZ2 inputs have a max of +/- 50mA input current, I have used it at double that at 1kHz. How does the real max input current scale with the PZT frequency? It it okay to use the full 100mA output continuously? 

Do you recommend switching to the LTC3331 for higher power?