Post Go back to editing

LTC4364-2 MOSFET M1 Failure

Category: Hardware
Product Number: LTC4364

Hi Team,

We are using LTC4364 IC in a surge protection circuit as given below.

V(IN): 48V

V(OUT): 48V upto 7.3A load

Selected MOSFET part number is marked in the given circuit image.

Surge Protector Circuit

The circuit works fine at the start but over a long run (say one or 2 months), we are facing MOSFET burning out issues. We cannot find the root cause of this issue.

Would you please look into it and direct us towards the solution?

Thanks,

Harish I I

  • Q1 needs the Safe Operating Area (SOA) performance to survive 4 situations:

    1. Start-up. Inrush current is controlled by slowly slewing Q1. Ease SOA stress using ENOUT to keep Load off until Cout is charged.
    2. Hard Short. (Current limit folded back to 50%)
    3. Soft Short. (100% Current Limit)
    4. Input Surge (Vin rises to max Vin during full load).

    There are previous posts detailing the calculations for these 4 points.
    Size the TMR cap to stay within the FET's SOA. 
    You can use LTspice to see the exact timeout in situations 2-4.

    I suspect the FET fails during start-up. Use the ENOUT feature.

  • When I observed the MOSFET failure, the PCB area around the MOSFET was black and seems to be delaminated due to heat. I think this kind of damage will not happen in an instant. It should be because of a prolonged stress. Hence, I cannot assume that the failure is at the start up.

    Also, we are testing with a resistive load and there is no Cout.

    So, what could be the possible reason for the failure?

    Could you please help us find the root cause.

  • When I observed the MOSFET failure, the PCB area around the MOSFET was black and seems to be delaminated due to heat. I think this kind of damage will not happen in an instant. It should be because of a prolonged stress. Hence, I cannot assume that the failure is at the start up.

    Startup is a common cause of failure, since there is VDS across the FET while the output cap charges and the load draws current. I*V=P.

    Also, we are testing with a resistive load and there is no Cout.

    I see 22uF of output cap in your schematic. Of course the resistor also contributes to stress during startup.

    So, what could be the possible reason for the failure?

    It's one of the 4 situations I posted.
    I suggest plotting these points on the FET's SOA graph.
    The FET needs to be able to survive each situation, and if it does, the FET should not fail.