Post Go back to editing

LTC4359

Category: Hardware
Product Number: LTC4359

Hello everyone,

I have a strange problem with the LTC4359CDCB, I hope someone can help me.
I am using the LTC4359 in three identical circuits connected in parallel on one board. I have used the schematic from the demo board DC1676A demo board, with only one difference, I used a different mosfet (SQJQ160E-T1_GE3).
Two circuits switch two batteries in parallel (23V) and an external switchable power supply (25V).

Now to my problem:
Above 20°C the circuit works as planned, but below 18°C only one circuit switches. Two circuits can be switched on a second circuit board.
If I only heat up the mosfet, the circuit works perfectly. The junction temperature of the mosfet is between -55 and +175°C and Vgs is 3V instead of 2V as in the example circuit.

I don't know exactly why the circuit reacts so sensitively to the temperature. Could a cold solder joint be causing the problem or does anyone have any other helpful ideas?

Regards

Patrick

  • If a circuit is temperature dependent, it could be a flux leakage issue. 
    Key areas to check are the SHDN# pin (which has a 10uA pullup), the GATE pin (20uA gate drive), and the components connected to these pins. High value resistors are significantly affected by board contamination.

    Touch up the solder joints in suspect areas, clean with IPA, and soak up the  residue with Kim wipes (or a paper towel).