Dear engineering team,
I'm designing an OR-ing schematic for OR-ing two power supplies: 48VDC tethered power supply, and 12S LiPo battery. I need to disable the battery if the tethered power is available till it drops to some UV limit, or is absent. In my first design, I used LTC4355, but the problem is that when the battery is fully charged ( 50.4V ), the system starts on battery, because its voltage is higher than of the tethered power supply. I don't want this to happen. So, I switched to LTC4372 as of the attached schematic. Please advice is that approach possible? If you have a better idea for solving the problem, please advice.
Thanks in advance with best regards
Nick