Post Go back to editing

LTM4671 - Figure 31, Vout1 (3.3V) configured correctly?

Category: Hardware
Product Number: LTM4671

In Figure 31 of the LTM4671 datasheet, both Vosns1+ and Vosns2+ are tied to the ‘3.3V’ output voltage.  Given the 13.3K feedback resistor, doesn't this result in a 2V output since the internal 60.4k resistors are in parallel and connected to the feedback resistor?  It seems like only one of the Vosns pins should be connected to the output voltage or the feedback resistor should be 6.65k to produce 3.3V.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.