I'm using EVAL-LT7170-AZ.
I want to set the output voltage of the LT7170 using a register. The set voltage target is 2.9V.

Therefore, from the resistance values of 107 kΩ (3.3 V) and 93.1 kΩ (2.5 V) listed in Table 7,
I calculated the intermediate voltage to be 100 kΩ (2.9 V) and implemented it on the evaluation board, but the output voltage was 3.3 V.
The datasheet states “1 Output voltage set point is controlled by VOUT_COMMAND”, but is it possible to set an output voltage that is not in this table by setting resistors?
Best Regards.