KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
LT3086
Recommended for New Designs
The LT3086 is a multi-feature, low dropout, low noise 2.1A linear regulator that operates over a 1.4V to 40V input supply range. Dropout voltage at 2.1A...
Datasheet
LT3086 on Analog.com
Hello,
I intend to use LT3086 as an adjustable voltage controlled current source as described on page 27 in the datasheet. What would be a correct equation für output current? Is that right: Iload=Vtrack/Rmon*1000?
Many thanks in advance.
Vitali Lach
Hi. I think your equation is correct. I show the equation and the reference design in the image below.

Thank you for that!
Best Regards.