Post Go back to editing

MAX20039 whistling

Category: Hardware
Product Number: MAX20039

I designed a CPU board with SMARC board and touch screen.

I am using the MAX20039 for the 12V backlight touch screen power supply. MAX20039 input is a 12.8 from battery.

The touchscreen have a pin ADJ to drive the brightness with PWM signal.

If the ADJ is place to 3.3V (without PWM), everything works well and the backlight is at 100%.

If I apply to ADJ a PWM (0 - 3.3V - 50%), the backlight is at 50%, but the CPU board generates an audible whistling sound.

Please find attached my schematics.

Parents Reply Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.