KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
MAX30102
Production
The MAX30102 is an integrated pulse oximetry and
heart-rate monitor biosensor module. It includes internal LEDs,
photodetectors, optical elements, and...
Datasheet
MAX30102 on Analog.com
MAX861
Production
The MAX860/MAX861 charge-pump voltage converters invert input voltages ranging from +1.5V to +5.5V, or double input voltages ranging from +2.5V to +5.5V...
Datasheet
MAX861 on Analog.com
Hello,
I am developing a smart wearable device featuring early detection and fall detection capabilities. Our current setup includes:
We found that the MAX30102 is not suitable for our application due to significant motion artifacts and its limitation to a single LED, which affects accuracy during wrist movements.
We are considering the MAX86174 as a potential PPG sensor for our project because of its multiple LED support and integrated accelerometer for motion artifact reduction.
Our key requirements are:
Challenges:
Our Questions:
We are eager to move forward with our development and would greatly appreciate any assistance or recommendations you can provide.
Thank you for your support.
Hi, Thank you for your inquiry.
A Non-Disclosure Agreement covers the product MAX86174 you are seeking support on, and we are unable to provide support for it in the public EngineerZone community. Per the Analog Devices EngineerZone Code of Conduct, we do not discuss NDA products on EngineerZone. To receive support on this product, please contact the CIC team.