For this component, I read in the datasheet that the maximum gate drive voltage is set by the voltage on VDDA. 
I am interested in the operation at voltages above 60V. I see in this image below that Vin is referenced to VDDA through a capacitor. So, I am wondering how the VDDA pin is setting the max gate drive voltage if VDDA is nearly at the same value as the source of M1 which is labeled as Vin. Based on my understanding, in order to properly drive M1 the maximum gate drive voltage should be around 10V higher than Vin (source pin of M1) (or what the VGS min of the FET is) in order for the mosfet to be driven on. Do you mind elaborating on how the proper gate drive voltage is produced for M1? And how it makes sure the voltage at the gate is higher than the source voltage to be sure that the mosfet is on? Thank you!