Post Go back to editing

Unable to get 1.5V Output Voltage

Category: Datasheet/Specs
Product Number: LT8624S

This is my design to get the 1.5V output voltage with input voltage of 12V and switching frequency of 500kHz. Supposedly I should get 1.5V at the output based on what the datasheet explain. But problem occurs when the output voltage is only 1.46V (400mV offset). Where does this 400mV go to? Also, does the PGFB pin will only be in the range of 462mV~537mV because I am unable to raise the voltage at that pin. Is there any ways to yield 1.5V output voltage?