Post Go back to editing

How to pump in 1V to VS+ from power supply for checking

Category: Hardware
Product Number: ADP1055

Hi All,

I connected 1v to VS+ from external power supply and connect VS- to AGND via 0ohm resistor. I did the READ_VOUT and there is reading almost close the Command out. And trim o VS+ can be done. However, I changing the value of Command OUT, does not adjust voltage accordingly. For example, at 12V output, 1 supplied 1V to VS+, then I change the command out to half to have output 6V, and meanwhile supplied 0.5V to the VS+. The output measured is still 12V.

So does it mean that I need to put a resistor from VS+ to VS- and connect a capacitor from VS- to GND ?

Please advice, thank you in advance.

Parents Reply Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.