Hello. I have a one question.
The LTM4657's Absolute Maximum Ratings for Vout is typically "-0.3V to 6V"
Is this specification valid even if no Vin is entered.
Best Regards.
LTM4657
Recommended for New Designs
The LTM4657 is a complete 8A step-down switching mode µModule (micromodule) regulator in a tiny 6.25mm × 6.25mm × 3.87mm BGA package. Included in the...
Datasheet
LTM4657 on Analog.com
Hello. I have a one question.
The LTM4657's Absolute Maximum Ratings for Vout is typically "-0.3V to 6V"
Is this specification valid even if no Vin is entered.
Best Regards.
The Vout maximums are valid, given all other pin voltages are sufficient for proper operation. Since this is a buck regulator, Vin must be sufficiently higher than the desired Vout so minimum off time is not violated.