Post Go back to editing

LTC7871 Constant Current into Hard Short

Category: Datasheet/Specs
Product Number: LTC7871

Can the LTC7871 configured as a buck converter in constant current mode operate into a hard short (<10mOhm)?

The DS references a "Current Foldback" graph that doesn't exist.

Will it have stability problems coming out of a hard short? And can the soft-start be defeated when the short is removed?

  • Hello Austin,

    I received your message. My comments are below:

    1. If a short is applied to VOUT which is strong enough to cause VOUT to fall out of regulation and the short is subsequently removed, then VOUT will ramp-up with internal soft-start. The supply will not have stability problems after the short is removed. The internal soft-start can not be disabled.

    2. For an LTC7871 supply configured as a constant current buck, the foldback current limit will cause the IOUT to be less than the IOUT programmed by the SETCUR pin if the foldback current limit is the lower of the two. Per the foldback charts inserted below (from page 9 of the D/S), the maximum current sense voltage progressively drops once the VFBLOW voltage falls below 0.4V. Therefore it VOUT is set for 14.0V nominal, for instance, then foldback will occur once VOUT falls below 4.7V. If the LTC7871 is being used to charge an automotive 12V battery, this should not be an issue.
       

     

    Best regards,

    Mike

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.