LTC4364
Recommended for New Designs
The LTC4364 surge stopper with ideal diode controller protects loads from high voltage transients. It limits and regulates the output during an overvoltage...
Datasheet
LTC4364 on Analog.com
Good day,

What are our current options?
Is there a way to make the turn-on time faster?
Speeding up start-up time and increasing inrush is not the answer to blown FETs.
Once you select the inrush current and assume max Vin, check if the HGATE FET has the Safe Operating Area (SOA) performance to survive start-up.
Which MOSFET would you recommend if we were to replace the SQJQ184E? We are very space-constrained. Should we look at a MOSFET with smaller input capacitance?
Small Ciss isn't important in hotswap applications, since we intentionally add Cgate for inrush control.
You want FETs optimized for SOA performance.
Here's an example of such a FET: PSMN3R7-100BSE
- The maximum expected current through the channel is 60 A, this will only occur once the MOSFET is switched completely on.
- The maximum turn-on current is 20 A.
Make sure the load is off until Cout is charged (Inrush=0A).
Otherwise, the load current is added to the SOA stress.
Use the ENOUT pin to signal the downstream load that start-up is complete.
Thank you for the response.


Make sure the load is off until Cout is charged (Inrush=0A).
Otherwise, the load current is added to the SOA stress.
Use the ENOUT pin to signal the downstream load that start-up is complete.
Regarding the SOA graphs, I'll refer you to this article about the Spirito Effect from the great Dan Eddleman.
https://www.analog.com/en/resources/technical-articles/mosfet-safe-operating-area-and-hot-swap-circuits.html
I'm skeptical because the SQJQ184E-T1_GE3 SOA curves are perfectly straight and in parallel.
There's no Spirito region, so I wouldn't trust its advertised SOA performance.
Thank you Ashapiro, this is really helpful. I will look into this article. Which MOSFET manufacturer would you say is trustworthy?
Thank you Ashapiro, this is really helpful. I will look into this article. Which MOSFET manufacturer would you say is trustworthy?