Post Go back to editing

MAX889resa+ IC- voltage dropping

Category: Hardware
Product Number: MAX889

In my design I have used MAX889resa+ IC which will convert positive voltage to negative voltage . In my design it will convert +3.3V to -3V with help of adjustable resistors . my load is 60 ohm , for this load voltage is dropping from -3V to 2.8V. But in data sheet it's mentioned it can handle 200mA load .Upto 200 ohm load the output voltage seems to stable without any dropout .  Why this IC  can't with stand this current ? why this issue is happening?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.