KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
LTC2955
Recommended for New Designs
The LTC2955 is a micropower, pushbutton on/off controller that manages system power by generating a clean enable output from the supply monitor input and...
Datasheet
LTC2955 on Analog.com
LT3060
Recommended for New Designs
The LT3060 series are micropower, low dropout voltage (LDO) linear regulators that operate over a 1.6V to 45V input supply range. The devices supply 100mA...
Datasheet
LT3060 on Analog.com
Hello,
I have the demo circuit 1836A with the LTC2955 on board, using default jumper settings out of the box.
If I power through VIN with a bench supply, everything works fine, no problems.
If I connect a Li-ion battery to VIN the device does not always power up correctly... often the LEDS just flicker and stay off, with no output on LDO.
Link to battery being used (ANSMANN 4S1P):
mister-battery.be/.../1194-pack-li-ion-18650-148v-26ah-m4a-r4-un-2447-3032-01.html
Battery voltage is 16.5 V so almost fully charged.
I can get the demo board to power up and run from the battery, but only after many attempts. Is there something I should be aware of in general when using Li-ion packs?
Kind Regards,
Anthony