LTC2955
Recommended for New Designs
The LTC2955 is a micropower, pushbutton on/off controller that manages system power by generating a clean enable output from the supply monitor input and...
Datasheet
LTC2955 on Analog.com
LT3060
Recommended for New Designs
The LT3060 series are micropower, low dropout voltage (LDO) linear regulators that operate over a 1.6V to 45V input supply range. The devices supply 100mA...
Datasheet
LT3060 on Analog.com
Hello,
I have the demo circuit 1836A with the LTC2955 on board, using default jumper settings out of the box.
If I power through VIN with a bench supply, everything works fine, no problems.
If I connect a Li-ion battery to VIN the device does not always power up correctly... often the LEDS just flicker and stay off, with no output on LDO.
Link to battery being used (ANSMANN 4S1P):
mister-battery.be/.../1194-pack-li-ion-18650-148v-26ah-m4a-r4-un-2447-3032-01.html
Battery voltage is 16.5 V so almost fully charged.
I can get the demo board to power up and run from the battery, but only after many attempts. Is there something I should be aware of in general when using Li-ion packs?
Kind Regards,
Anthony
I tried powering DC1836A-A from my batteries and I could not replicate the problem you are seeing. My battery packs make around 18VDC. Hot-plugging an input supply can cause voltage overshoot that can cause electrical stress-type damage, but I am not sure why hot-plugging would cause intermittent operation. 
The issue is related to the BMS of the battery pack I am using, I managed to reduce the voltage transient using electrolytic capacitors, but then the issue of inrush current also causes the BMS to cut off the battery from the load.
So, I need to do further design work to also limit the inrush current and prevent the BMS from "tripping".... but that is a different issue, not related to the eval board :-)
The issue is related to the BMS of the battery pack I am using, I managed to reduce the voltage transient using electrolytic capacitors, but then the issue of inrush current also causes the BMS to cut off the battery from the load.
So, I need to do further design work to also limit the inrush current and prevent the BMS from "tripping".... but that is a different issue, not related to the eval board :-)