Post Go back to editing

Power up issue when using Li-ion battery - DC1836-A (LTC2955)

Category: Hardware
Product Number: LTC2955

Hello,

I have the demo circuit 1836A with the LTC2955 on board, using default jumper settings out of the box.

If I power through VIN with a bench supply, everything works fine, no problems.

If I connect a Li-ion battery to VIN the device does not always power up correctly... often the LEDS just flicker and stay off, with no output on LDO.

Link to battery being used (ANSMANN 4S1P):

mister-battery.be/.../1194-pack-li-ion-18650-148v-26ah-m4a-r4-un-2447-3032-01.html

Battery voltage is 16.5 V so almost fully charged.

I can get the demo board to power up and run from the battery, but only after many attempts. Is there something I should be aware of in general when using Li-ion packs? 

Kind Regards,

Anthony



added tag per member request
[edited by: GenevaCooper at 3:00 PM (GMT -4) on 6 Aug 2024]
Parents
  • Update:

    My issue appears to be related to voltage transient on connecting the battery, as I have no circuitry in-between the battery and the Eval board. See attached trace, battery voltage spikes to around 28 V on connecting (nominal 16.5 V as charged). 

Reply
  • Update:

    My issue appears to be related to voltage transient on connecting the battery, as I have no circuitry in-between the battery and the Eval board. See attached trace, battery voltage spikes to around 28 V on connecting (nominal 16.5 V as charged). 

Children
No Data