Post Go back to editing

Power up issue when using Li-ion battery - DC1836-A (LTC2955)

Category: Hardware
Product Number: LTC2955

Hello,

I have the demo circuit 1836A with the LTC2955 on board, using default jumper settings out of the box.

If I power through VIN with a bench supply, everything works fine, no problems.

If I connect a Li-ion battery to VIN the device does not always power up correctly... often the LEDS just flicker and stay off, with no output on LDO.

Link to battery being used (ANSMANN 4S1P):

mister-battery.be/.../1194-pack-li-ion-18650-148v-26ah-m4a-r4-un-2447-3032-01.html

Battery voltage is 16.5 V so almost fully charged.

I can get the demo board to power up and run from the battery, but only after many attempts. Is there something I should be aware of in general when using Li-ion packs? 

Kind Regards,

Anthony



added tag per member request
[edited by: GenevaCooper at 3:00 PM (GMT -4) on 6 Aug 2024]
Parents
  • To add:

    Looking at the schematic, there is an LT3060 on board to power the LED's. Input capacitance is 1 uF and output capacitance is 2.2 uF, I'm wondering if this is causing the issue when powering from battery?

    When using a bench supply the input voltage is ramped up more slowly, compared to connecting the battery terminals.

    For reference I found this post which explains:

     RE: LT3060 output capacitor 200uFx2 

    I notice that the LTC2955 enable output does not latch if I disconnect the LT3060, maybe in this case I have to remove R15 & R18 which connect to U7 (LT6700)?

    Kind Regards,

    Anthony

Reply
  • To add:

    Looking at the schematic, there is an LT3060 on board to power the LED's. Input capacitance is 1 uF and output capacitance is 2.2 uF, I'm wondering if this is causing the issue when powering from battery?

    When using a bench supply the input voltage is ramped up more slowly, compared to connecting the battery terminals.

    For reference I found this post which explains:

     RE: LT3060 output capacitor 200uFx2 

    I notice that the LTC2955 enable output does not latch if I disconnect the LT3060, maybe in this case I have to remove R15 & R18 which connect to U7 (LT6700)?

    Kind Regards,

    Anthony

Children
No Data