Hello,
Is there an evaluation board available for the MAX16151, or equivalent / similar part?
Kind Regards,
Anthony
MAX16151
Recommended for New Designs
The MAX16151 is a high voltage, pushbutton on/off controller with a switch debouncer and built-in latch. This device accepts a noisy input from a mechanical...
Datasheet
MAX16151 on Analog.com
Hello,
Is there an evaluation board available for the MAX16151, or equivalent / similar part?
Kind Regards,
Anthony
Hello Anthony,
for MAX16151 is there unfortunately no Eval-Board.
You can surely order samples.
There are other number of push-button controllers, which are high voltage (Vcc>5V) and have eval boards.
A short list below.
Add after analog.com
www.analog.com/en/parametricsearch/12984#/p5346=1.5V%20to%2036V|2.7V%20to%2026V|2.7V%20to%2027V|2.7V%20to%2028V|5V%20to%2036V&d=s8|s6|s7|s25|s3|s5|165|5346|5576|5575|3942|5343
I hope these or MAX16151 samples help.
Hello,
Thank you, I have ordered an eval board for the LTC2955 which should be OK. DC1836A.
Kind Regards,
Anthony