Are the following FETs compatible with the LTC4444-5 driver:
- ROHM RQ5L030SN, NFET 3A 60V SOT-346T
- Vishay SQS850EN, VDS (V) 60 RDS(on) = 21mΩ at VGS = 10 V ID = 12A\
Please if you could provide some feedback
Thank you.
Fausto Bartra
LTC4444-5
Production
The LTC4444-5 is a high frequency high voltage gate driver that drives two N-channel MOSFETs in a synchronous DC/DC converter with supply voltages up to...
Datasheet
LTC4444-5 on Analog.com
Are the following FETs compatible with the LTC4444-5 driver:
Please if you could provide some feedback
Thank you.
Fausto Bartra