Hello,
I am working on a voltage rail and I would like to use the LT3083 (TO-220) for this application. The worst-case supply voltage is 27V and the output voltage of the LT3083 will be set to 19.25V. The output of the LT3083 cannot be shorted in this application and the input/output voltage differential will be 27 – 19.25 = 8V maximum.
In the spec sheet I find following specifications:
CONTROL Pin Voltage.............................................±28V
IN Pin Voltage (T5, Q Packages) ....................18V, –0.3V
No Overload or Short-Circuit .....................23V, –0.3V
On page 28 of the spec sheet there is a sample circuit of the LT3083 running in parallel. This circuit has an input voltage of 4.8V TO 28V.
I would like to know if the Vin pin of the LT3083 can handle the 27V input voltage?
If not, is a workaround possible where I limit Vin to 23V max during start-up and when the output voltage exceeds for example 12V to increase Vin to the 27V max?
Edit Notes
Added LT3083 to title[edited by: Ruthlesstheone at 1:53 PM (GMT -4) on 18 Jul 2024]