Post Go back to editing

Transient Output voltage simulation

Category: Hardware
Product Number: LTM8068

Dear Engineers,

I have an issue with LTM8068 DC/DC converter, that is as i  run tranisent simulation with input of 28VDC 

given that I choose the resistors values as specified in the datasheet, the output doesn't settle at 5V 

it increase to higher values with transient time is 50ms.

ltm8068_test.asc

  • Hello Nawaf,

    the LTM8068  requires a minimum load to stabilize the output voltage. See the corresponding chapter on page 14 and the correspondig graph on page 6 of the datasheet.

    In your simu, you have not load at all at the output. Add the required minimum load (e.g. 500 Ohm between Vout1 and VoutN), and the output will stabilize at the intended voltage.

    best regards

    Achim

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.