LTC4414
Recommended for New Designs
The LTC4414 controls an external P-channel MOSFET to create a near ideal diode function for power switchover. This permits highly efficient OR’ing of...
Datasheet
LTC4414 on Analog.com

In figure 7, SENSE is connected to ground to fully enhance the PFET when CTL goes high.
You have SENSE connected it to VOUT, which is only useful in a diode configuration (LTC4414 regulates VFWD to block reverse current).
Try connecting SENSE to ground.
Thanks for your answer.
The failure don't happen to all device but just in some of them? Do you think it can be the reason?
It is very difficult to reproduce problem...but apparently it happen randomly. This is the reason that even if I will connect Sense to GND., I will not known if it fixed the problem.
BTW, what about the parallel PFET connection. Is it OK?
Thanks
Aharon
The failure don't happen to all device but just in some of them? Do you think it can be the reason?
Maybe. Could be an safe operating area (SOA) issue if COUT is big and the load is connecting during start-up.
BTW, what about the parallel PFET connection. Is it OK?
Paralleling FETs is okay, but if you want to increase current handling, why not just switch to an NFET controller?
You'll get the ability to control inrush current into COUT during start-up, which would address an SOA issue.
Look into the LTC4365 and LTC7004.