Post Go back to editing

SHTD# leads to much slower Gate discharging than specified

Category: Hardware
Product Number: LT4363-2, LT4363

Hi there,

we experienced that in our circuit the MOSFET got burned when using SHTD# to switch off.

According to datasheet and  LT4363IDE-2 FET gets in short  the Gate should be discharged with 1mA. But this is only the case until the Gate-voltage is down to the output voltage. After that the Gate discharging gets extremely slow. We confirmed that by using the ADI evaluation module (https://www.analog.com/en/resources/evaluation-hardware-and-software/evaluation-boards-kits/dc1935a-b.html ).

We modified the board by desoldering the 47nF CG cap, in order to accelerate Gate charging/discharging as much as possible.

We connected a 2A load and switched on and off using the SHTD# pin. The Gate-voltage was charged to 25V (13V above Vin), discharging needed 13us for 15V Gate-voltage-drop - this should be OK for 1mA discharging current and only the input capacitance of the FET. After the 13us the Gate voltage droped down way slower (see osci screenshot). It never dropped below the output voltage, which in turn resulted in bad output voltage drop.

(black: SHTD#; green: Gate; red: output
note different scaling!)

BTW: We saw the same behaviour when using UV as switching input.

I think this is an undocumented behaviour, isn't it? Our interpretation: for switching the MOSFET on/off by SHUTD# needs a MOSFET with very relaxed SOA specification - which comes with quite a big package. In *our circuit* voltage und current are higher (30V/30A). Our MOSFET would survive the discharging if it were done with 1mA - but this timing is so bad that we would need a MOSFET that does not fit to our PCB.

Is there any modification possible to ensure 1mA Gate discharging down to 0V completely ?

In case we would discharge the gate with an external NPN transistor (controlled by inverted SHTD#) - would this lead to any issues in the LT4363-2 (e.g. overload to the charge pump)? Should we use a series resistor then?

Thank you in advance!

  • we experienced that in our circuit the MOSFET got burned when using SHTD# to switch off.

    According to datasheet and  LT4363IDE-2 FET gets in short  the Gate should be discharged with 1mA.

    When pulling SHDN# low, IGATE(DN) is 1mA (typ), but can be as low as 0.05mA.

    But this is only the case until the Gate-voltage is down to the output voltage. After that the Gate discharging gets extremely slow.

    When VGATE=VOUT, VGS=0, and FET is off.
    GATE is just following OUT as it decays.
    If you have red and green traces at the same scale and reference point, this will be more obvious.

    If using the LT4363 as a switch, you may get a low gate pulldown current and be stuck in the linear region for longer with max load current flowing.
    For faster switching, consider the LTC7003 or LTC7004.

  • Thanks a lot. A colleage also pointed me to the mistake regarding Vgs.

    Another mistake was that the load was resistive, not constant current. I should have analysed better.

    Thank you also for recommending the LTC700x - I guess there is no fast switch with current *limiting* (not overcurrent protection) ... and temperature range starting from -55°?

  • Check out the LT4356 with MP temperature grade.
    It has milliamps of gate pulldown.

    It also has active current limiting.