Post Go back to editing

LTC4355 and Mosfet in parallel

Category: Hardware
Product Number: LTC4355

Hi, I use LTC4355 for a power distirubuter project. I use two mosfet for power switch IN1 and IN2 in my design (SIJ186 - MOSFET N-CH 60V 23A). The mosfet heats up in high current rating above 10A. Can I connect two or more parallel mosfet both IN1 and IN2. For example two parallel mosfet for IN1 and also two for IN2. Can I drive two or more mosfet from gate1 or gate2

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.