Post Go back to editing

MAX16165ATPH T

Thread Summary

The user identified two errors in the calculations for selecting feedback resistors and offset current for the SET pin: R_ios should be 100 kΩ instead of 10 kΩ, and the correct formula for R_2 is R_2 = R_1 × 0.5 / (V - 0.5V). The support engineer confirmed the corrections and provided an updated calculation diagram.
AI Generated Content
Category: Datasheet/Specs
Product Number: MAX16165ATPH+T, MAX16165

Selecting SET_ Feedback Resistors and Offset Current

While tunning resistors values for SET pin I notice two errors: 

  1. The R_ios resistor value in the calculations is wrong, it should be 100 Kohms instead of 10 Kohms
  2. The formula for calculating R_2 is wrong, in the first occurrence, the formula is: R_2 = R_1 × 0.5 / _ but below the formula is R_2 = R_1 × 0.5 / (_ - 0.5V).

According to this, after testing the IC the good formula is the second one

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.