I have an application with generic IO pins configurable as either voltage, 0~10VDC, and current loop, 4~20mA, inputs. The voltage input is always low-current, i.e. <20mA, so I was hoping to use the MAX14626 as a common protection device for the input pin regardless of it's configuration. I have the IC hooked up as indicated on the datasheet, but when I apply my external voltage input to pin 1 of the MAX14626 I see the output, pin 6, jump up to 1.3VDC and just sit there independent of the input voltage. What am I doing wrong?
The load resistance connected to IC GND from pin 6 is 500Ohms which should give me a full 0~20mA over the full input voltage range of 0~10V. My understand was that the MAX14626 is fundamentally a pair of back to back FET switches controlled to provide 30mA maximum current limit -- obviously I am missing something. Any ideas?
Thanks!
~Jon