Post Go back to editing

LTC4267-3 does not start switching

Category: Hardware
Product Number: LTC4267-3

Hello,

I just received some new custom PCBs with PoE controller LTC4267-3.

I already used the same circuit on another PCB before, only with small modifications, mainly now with another Rclass resistor = 45R3 for class 3.

At first the LTC "registered" with the PSE, but after about 500 ms power was turned off.
The problem: the LTC does NOT start switching.

I added a 10k resistor load (Vportp and PGND), now the PSE keeps the input power up, but still no switching action.

The voltage level at ITH/RUN pin is about 0.55V.

I have changed the FET (controlled by nPWRGOOD, also checked that) at ITH/RUN, several resistor values, no success, no switching!

Any ideas?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.