Post Go back to editing

While making an external short, the component mosfet does not disconnect

Category: Hardware
Product Number: LT1910

hello ,

LT1910 

       1. I don't quite understand, for this there is the diode that will bypass the capacitor during discharge?

  1. I need charging controlled by a capacitor/resistor around these values and that is normal for slew rate.
  2. But when I perform a short on the EFUSE (Mosfet Q8) port it does not function and drops the internal voltage 8.2v to 0V.
  3. Do I need a specific diode in the data sheets, they use 1N4148 and this is what I use, maybe I need a Schottky or FAST RECOVERY diode?
  4. Even if I put a 10NF capacitor in C235, and a 4.75K on R155 and on R157 value 10 ohm, It still does not work.( see sch diagram) even after I removed the capacitor C235 the voltage internal dropped, 8.2v to 0V.
  5. I don't see this phenomenon in the simulation as I check on the card ?
  6. Rsense is 0.007 mOHM (R64 see DWG)

Note : Only use "control network "

Thread Notes

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.