LTC7890
Recommended for New Designs
The LTC7890 is a high performance, dual step-down, dc-to-dc switching regulator controller that drives all N-channel synchronous gallium nitride (GaN)...
Datasheet
LTC7890 on Analog.com
Hello,
I am having issues with the LTC7890 GaN-FET controller configured in a two-phase setup and operating as a current source to drive a diode load. The dev board with EPC FETs was reconfigured for such an application and was successfully implemented into the prototype design. Please see the attached schematic to understand the working principle and connections.
The issue is that with the new prototype board, two of GanSystems FETs are used for the high side, and the SW1 node is being damaged easily.
Tests Conducted:
Initially, I suspected Cboot, so I increased it from 100n per phase to 2.2u and later added a 4.7-ohm resistor to remedy transients. However, this did not help.
Switching frequency does not affect the failure. With a DC setpoint voltage fed into the ITH1 pin, the frequency was swept up to 2MHz, and the device continued to function. With feedback connected and fsw set to 500KHz, it continued to fail.
Attached are the following for reference:

Any insights or suggestions on what might be causing this issue would be greatly appreciated.
RokJas Did you manage to solve the problem? I have encountered a similar problem and am looking for a solution.
Unfortunately I did not. I have continued testing with a single FET on the high side and it seemed to be enough for my application.
I was able to solve the problem, but I don't know what the source is. Increasing the switching frequency in my case helped.