Post Go back to editing

LT8362 output voltage dropping under load

Category: Hardware
Product Number: LT8362

I'm trying to build a step up converter to for from 6.5-8.3V DC all the way up to 48V with a maximum load of 15W.

I've gone with SEPIC configuration of an LT8362.  I've gone with SEPIC over boost only to allow the output to be switched off completely.
My schematics attached below.

The problem I have is this, at no load Vout is a nice 48V, however as the load on the output goes above 2W, Vout drops back down to about 20V.  Is someone able to give me some tips on what I can do to try an diagnose and resolve this problem?.

  

 C3, C11 Ceramic Capactior 1206 1uF 100V X7R Samsung CL31B105KCHSNNE
    C10 Ceramic Capactior 4.7PF 100V C0G/NPO 0603 YAGEO CC0603CRNPO0BN4R7
    C12 Ceramic Capactior 0603 10nF 16V X7R  YAGEO CC0603KRX7R7BB103
    C14 Ceramic Capactior 0603 1nF 100V X7R  Samsung Electro-Mechanics CL10B102KC8NNNC
 R1, R2 RES 1M OHM 1% 1/10W 0603 Stackpole Electronics Inc RMCF0603FT1M00
R4-R6, R8 RES 34K OHM 1% 1/10W 0603 Stackpole Electronics Inc RMCF0603FT34K0
 R7, R9 RES 0 OHM 1% 1/10W 0603 YAGEO AC0603JR-130RL 
    Q2 0.17A Id, 100V Vds, N-Channel MOSFET, SOT-23   BSS123-7-F
 C1, C2, C4-C9 Ceramic Capactior 0603 4.7uF 100V XR7 KYOCERA AVX 12101C475K4T2A
    U1 Switching Voltage Regulators Low IQ Boost/SEPIC/ Inverting Converter with 2A, 60V Switch Analog Devices LT8362EDD#PBF
    L1 INDUCT ARRAY 2 COIL 15UH SMD Bourns Inc. SRF1260-150M
    D1 Diode Schottky 150 V 1A Surface Mount SOD-123FL SMC Diode Solutions DSS115UTR
    Q1 MOSFET P-CH 30V 8A 6TSOP Vishay Siliconix SI3421DV-T1-GE3
    F1 FUSE 0603 6A , 70A In rush current AEM F0603HI6000V032TM 
Parents Reply Children
No Data