Post Go back to editing

LT3762

Category: Hardware
Product Number: LT3762

Hi we have a replication of demo board of LT3762 but have a problem when apply VIN lower 11 Vdc, i set circuit to 25V and 1A output to led string.

The problem have when Vin are low8-12 Vdc, i set En/UVLO with 49k and 49k. when power the ic have hight temperature and not work led string

Can you help me

Thank

this are schematic with VIN 5/6 Vdc and string led 20V / 1A

Edit Notes

Schematic
[edited by: ulis at 11:55 AM (GMT -4) on 27 May 2024]