Post Go back to editing

Can the LTM4651 support a spread-spectrum input clock?

Thread Summary

The user asked if the LTM4651 can support a spread-spectrum input clock from the LTC6909. The LTM4651 can accept a spread-spectrum clock as long as the CLKIN frequency is within ±40% of the oscillator frequency set by the fset pin. No specific parameters beyond this tolerance were mentioned.

View FAQ
AI Generated Content
Category: Hardware
Product Number: LTM4651

Can the LTM4651 support an input CLKIN signal that incorporates spread-spectrum frequency shifting?

More specifically, can it support the spread-spectrum input clock from the LTC6909?

If the the LTM4651 can accept a spread-spectrum clock input from the LTC6909, are there any specific required parameters?

Thanks in advance,

Chris

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.