Hi,
we have designed a board with ADP5070AREZ-R7 regulator. We had referred to the datasheet and created the design using the ADP507x_Designer_Release.xlsm.
Now, when we are testing the same, we are unable to get 11V at the outputs (+11V & -11V).
Can someone help me with this? What could be wrong here?

Details:
Input : 6V (6A max)
Outputs:
SW1 : +11V (designed for 200mA)
SW2 : -11V (designed for 110mA)
Observations: The positive voltage is coming as 0V and the negative voltage is observed to be swinging from 1V to 5V.
Thanks in advance.
Regards,
Nanjunda M