Hello
I was wondering if someone could help with the terminology on datasheets
When I look at the datasheet for the LT8362, it states that INTVCC draws power from the BIAS pin if: 4.4V ≤ BIAS ≤ VIN
I'm guessing it means that if that voltage on the BIAS pin is between 4.4V and VIN. Then the LT8362 will take the input voltage from the BIAS pin instead of VIN
Is this correct? If not please clarify
Thank you