Post Go back to editing

Vin 12-36V Vout 2.5V/100A

Category: Hardware
Product Number: LTC7871

Hi. Has anyone built applications on the above-mentioned IC with the given parameters as in the topic? I wonder if it will work stably and if it is possible to obtain 2.5V at the output and 100A at an output voltage of 12-36V. The application provides an input voltage range of 30-70 and an output voltage of 12V/180A. Theoretically, 2.5V is possible, but is it really?