Post Go back to editing

LTC3261 not generating negative output.

Category: Hardware
Product Number: LTC3261

LTC3261 not generating negative output voltage with input of 15V.

Circuit designed as per datasheet.

OUTPUT VOLTAGE IS 1.27V 

Load Condition is No Load

Parents
  • Hello, 

    Looks like the output is being pulled positive for some reason. I have seen when the output is connected to the negative of an op amp the positive voltage passes thru the op amp and pulls the output voltage positive. With no load it should not be positive. Is it possible to tell if the EPAD is soldered well? This serves as the GND for the IC. The only other suggestion is to check the solder connections. The only thing missing on the schematic is the input capacitor. That should be placed between VIN and GND and close to the part. Below is a recommended layout from the datasheet. 

Reply
  • Hello, 

    Looks like the output is being pulled positive for some reason. I have seen when the output is connected to the negative of an op amp the positive voltage passes thru the op amp and pulls the output voltage positive. With no load it should not be positive. Is it possible to tell if the EPAD is soldered well? This serves as the GND for the IC. The only other suggestion is to check the solder connections. The only thing missing on the schematic is the input capacitor. That should be placed between VIN and GND and close to the part. Below is a recommended layout from the datasheet. 

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.