Post Go back to editing

Modifying DC1521A to operate LT3956 in buck / boost mode

Category: Hardware
Product Number: LT3956

I am looking for a WLED driver that can meet the following requirements and I believe the LT3956 would work:

  • VIN: 12VDC-48VDC
  • Vf_max for LEDs: 18.5V
  • I_led max: 1.4A
  • Analog dimming

I have ordered the evaluation board to test it out. The eval kit manual says that "Modifications can be made to the DC1521A in order to convert the board from a boost topology LED driver to any other topology".

Is it possible to get instructions on how to modify the evaluation kit to support a buck/boost operation to the above parameters?

Thanks,

-Mike

Parents
  • I updated the provided simulation to match the buck boost reference schematic from the datasheet and I'm unable to run the device in buck/boost with an input of 48V. It appears that the voltage is exceeding 80V on the ISP pin which seems to cause the model to stop switching.

    Before I blow up my evaluation board is this expected behavior? It seems this part is not suitable for this application then.

Reply
  • I updated the provided simulation to match the buck boost reference schematic from the datasheet and I'm unable to run the device in buck/boost with an input of 48V. It appears that the voltage is exceeding 80V on the ISP pin which seems to cause the model to stop switching.

    Before I blow up my evaluation board is this expected behavior? It seems this part is not suitable for this application then.

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.