I am looking for a WLED driver that can meet the following requirements and I believe the LT3956 would work:
- VIN: 12VDC-48VDC
- Vf_max for LEDs: 18.5V
- I_led max: 1.4A
- Analog dimming
I have ordered the evaluation board to test it out. The eval kit manual says that "Modifications can be made to the DC1521A in order to convert the board from a boost topology LED driver to any other topology".
Is it possible to get instructions on how to modify the evaluation kit to support a buck/boost operation to the above parameters?
Thanks,
-Mike