Hello, can I connect the output of your AD8561 hysteresis comparator directly to the VSW pin of the MAX5097 buck converter if I want to use a hysteresis comparator to control the switching diode off and on in a buck converter ?
Help me,please!

MAX5097
Production
The MAX5096/MAX5097 easy-to-use, Dual Modeâ„¢, DC-DC converters operate as LDO (low dropout) or switch-mode buck converters. At a high output load, the...
Datasheet
MAX5097 on Analog.com
AD8561
Production
The AD8561 is a single 7 ns comparator with separate input and
output sections. Separate supplies enable the input stage to be
operated from ±5 V dual...
Datasheet
AD8561 on Analog.com
Hello, can I connect the output of your AD8561 hysteresis comparator directly to the VSW pin of the MAX5097 buck converter if I want to use a hysteresis comparator to control the switching diode off and on in a buck converter ?
Help me,please!