KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
MAX160
Production
The MAX160 and MX7574 are low cost, microprocessor compatible 8 bit analog-to-digital converters which use the successive-approximation technique to achieve...
Datasheet
MAX160 on Analog.com
MAX16046
Production
The MAX16046/MAX16048 EEPROM-configurable system managers monitor, sequence, track, and margin multiple system voltages. The MAX16046 manages up to twelve...
Datasheet
MAX16046 on Analog.com

Hello SamLi,
I wanted to let you know that I tried to install the software on a terminal running Windows 11 operating system and the installation was successful.
See snipped photos are attached.
There is also a black area in the software that appears the same as when it is installed on a terminal running Windows 10 OS.
I am currently working on obtaining the evkit and testing its ability to read the registers.


regards,
Chris
Hi SamLi,
This is to confirm that the GUI software is working the same for windows 11, the black area of the GUI is enabled and can be reconfigure. it changes it's color once you hover the mouse on specific table row. I attempted to load the MAX16046 EV Kit Demo.xml file but couldn't observe the voltage readings. You may need to adjust settings and configure according to your needs to enable voltage data logging.
I haven't get any response from this thread, I'll consider this inquiry closed.