Post Go back to editing

LTC4263 - 1000Mbps Design

Category: Hardware
Product Number: LTC4263

Hello,

We have a device in our product that can be powered over PoE with 1000Mbps of data flow and are looking into a PSE controller that can do it.

The LTC4263 looked very interesting and might be a solution, but I'm not quite sure on how or if this is the correct part for implementation (if it should be a different part then if a suggestion could be made that would be great).
I do have a couple questions regarding this:

1. This sounds like a general question, but can PoE still negotiate and operate at 24V? I want to avoid using a DC/DC regulator to bump it to 48V. Not sure if a PoE injector IC of sorts is needed here.
2. If I was to implement this with 1000Mbps data speeds (using all 8 pairs), which center taps would power need to be connected to? As I understand, it would be between CT of pairs 1&2 and 7&8. In the same respect, we would be using a custom connector where we expect power to flow with data and would be provided on a separated contact point.
3. Is the evaluation board for this chip only compatible for 100Mbps devices as power flows through the spare pins?

Any help on any of those questions and/or links to where the answers may lie would be greatly appreciated!

Kind Regards,
Neehar