Post Go back to editing

Question for ADP2371's LTspice model

Thread Summary

The user encountered an issue with the ADP2371-ADJ LTspice model where the circuit fails to switch and reach the target output voltage (5V) when FSEL is set to Low (GND, fsw=600kHz). The final answer confirms the problem and suggests sharing the simulation file for further investigation. The accompanying answer requests the simulation file to diagnose the issue.
AI Generated Content
Category: Software
Product Number: ADP2371
Software Version: LTspice XVII / 24

Hello ADI support,

I  am simulating on ADP2371-ADJ 's LTspice model.
It can work at FSEL=High=Vin(fsw=1.2MHz), however it can not work at FSEL=Low=GND(fsw=600kHz).
Is it rooted by LTspice's internal model issue ?

Regards,
Yuta Ueno / Marubun FAE

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.