Post Go back to editing

LTC4227 operation with dual 2S battery

Category: Hardware
Product Number: LTC4227

Hello,

I am working on design where we have redundant battery inputs. I am using a dual bench power supply set at 8.4V both channels representing two 2S fully charge lipo batteries and connected at IN1 and IN2 of the LTC4227.

#D2ON threshold is set to 6.4V for IN1 using a voltage divider

ON pin threshold is set to 6.2V at Sense+ using a voltage divider.

According to the above I was expecting the LTC to switch at IN2 when the IN1 reach the 6.4V (D2ON threshold), but when I start decreasing the IN1 voltage and reach a voltage of 7.8V then the LTC  switch to IN2.

Did anyone face that before?  LTC4227 switch to IN2 when IN1 has 0.6V less than IN2?

Below our schematic

Thank you,

Alexis Kyriakou



Schematic added
[edited by: AlexisKyriacou at 2:04 PM (GMT -5) on 23 Feb 2024]
Parents
  • Did anyone face that before?  LTC4227 switch to IN2 when IN1 has 0.6V less than IN2?

    The key is the 0.6V figure - It's a diode drop.
    Q1 and Q2 form a diode-OR, where the higher supply is passed to the output.
    Even if you use the D2ON# feature, the diode-OR behavior will still occur due to the body diodes of Q1/2.

    I believe the intent of the pin is to disable VIN2's ideal diode and prioritize VIN1.
    This works as long as the VSD across Q2 is <0.6V.

Reply
  • Did anyone face that before?  LTC4227 switch to IN2 when IN1 has 0.6V less than IN2?

    The key is the 0.6V figure - It's a diode drop.
    Q1 and Q2 form a diode-OR, where the higher supply is passed to the output.
    Even if you use the D2ON# feature, the diode-OR behavior will still occur due to the body diodes of Q1/2.

    I believe the intent of the pin is to disable VIN2's ideal diode and prioritize VIN1.
    This works as long as the VSD across Q2 is <0.6V.

Children